Hi
This is Raja, i am using LMZ23610 as regulator module for driving 3.9V (10 A ) load . But when i drive 3.9V (9A) Power LED, it getting more heat at the amp of 3A . here voltage is reduced from 3.9V to 2.9V .
And then am increase the output voltage 3.9V to 4.5 V by changing the resister combination , it drives 5A load , here the voltage dropped from 4.5 to 3.2V and the module getting more heat ....
can anyone give me the solution for that ?