Hello
I am using PTH04T241WAD for powering the FPGA.
10 capacitors are connected to its output.
Each capacitor is 100uF, ESR=2mOhm (GRM32ER60J107M MURATA).
How should I correctly define the capacitor's type (Type A or Type B or Type C) for operating in the TurboTrans mode?
What is "C" in the (C х ESR) formula? Is it the total output capacitance or the capacitance of the individual capacitor?
So, what of the following is correct?
10 х 100uF х 2mOhm = 2000 - Type B
or
100uF х 2mOhm = 200 - Type A ?
Best Regards
Alex