Hi all,
We found that two units DCP021212DU were borken, and sent back to TI PWR business for analysis.
Both units were decapsulated, they found that exposed copper windings with missing wire coating.
Both units failed as a result of a short from primary to secondary windings on the transformer.
(Please refer to attachment).
They think that degradation of the magnetic wire varnish can occur if the DCP02 is exposed to a high humidity environment followed by high temperature exposure, such as solder re-flow.
About the humidity issue, we got 1K pcs DCP021212DU on 9 September 2013, and sent to the manufacture factory on 10 September 2013. Before soldering, they didn't open the bag in the manufacture factory. The time that DCP021212DU touched air should less than 12 hours.
Question: There are still 800 pcs semi-products in our company, we have to check these semi-products were degraded or not? Besides Laser ablation de-capsulation, how to find out exposed copper windings with missing wire coating?
<PS> We try to use high resistance meter (2000Mohm/1KV and 200Mohm/500V) to measure the resistance between primary to secondary. We test 10 pcs samples, the resistance between primary to secondary of these 10 pcs are all greater than 2000M ohm. High resistance meter can't find out degraded parts.