This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCR010505 question

Other Parts Discussed in Thread: DCR010505

I'm testing the DCR010505 and came across the following problem. I tried the basic circuit and without a load the output is 5.02V and the ripple is around 5mV (measured with the myDAQ).

When I turn the load there is a drop and the output is around 4.27V and the error pin goes to the low state.

Trying to solve this problem I put a ceramic capacitor of 100nF between the 0V pin and the isolated ground (this pin was direct connected to the isolated ground). And this solved the problem. With the load the Vout is around 4.99V and the ripple around 15mV.

But why? (I'm using a breadboard to the test).