Hi all,
we use the LMZ23610 in several different boards with output voltages from 1.2V to 5V. After soldering (vapour phase, 2 different furnaces), some of the LMZ parts have shorts at the output and sometimes at the input, too. If I apply an input voltage, most of them work and the short disappears. At some parts the short does not disappear. Other parts have a wrong output voltage - the feed back voltage is not 0.8V in such a case. Some parts are too low (FB voltage is 0.5V, for example) others are too high. We bought these parts at Farnell in June 2014. At the moment I have 5 parts (of 20) with problems. We have approx. 7 years experience with the vapour phase systems and all other PCBs - even if soldered twice (top bottom) do not show problems. So I assume that this should not be the reason for our problem.
The schematic is more or less a copy of the datasheet (FB resistors, capacitors,...), we have 2x330uF output capacitors + 22uF + 47nF ceramic, etc.
Is there a known problem (soldering, bad parts delivered in June,...)
Does anybody has an idea?
Thanks
Martin