I am trying to use the inhibit pin to disable the regulator output to save power on my system. I have a PTN78020W on two boards and they are both having the same issue.
The problem is that when I bring the inhibit pin to ground the output does not fall to 0VDC but about 1.6VDC. I have tried 3 different methods to bring the inhibit to ground, none of which turn the PTN78020W completely OFF.
First, I pull the inhibit pin to ground using an I/O pin on a STM32F407 micro-controller. Based on the PTN78020 datasheet I would expect the low level ground signal from the micro to pull the inhibit pin down.
Second I placed a N-FET from the inhibit pin to ground as shown in the datasheet example. I use the STM32F407 to drive the gate and also directly connected the gate to 3.3VDC to turn the N-FET ON and both had the same outcome.
Lastly I shorted the inhibit pin to ground and did not see the regulator output fall to zero, it's output was about 1.6VDC.
I am not sure what is happening here and I have run out of ideas.
I have a 4.7uF input cap and the following values on the output, 220uF tant, 100uF tant & 1uF. The ADJ pin is connected to a digi-pot so that i can trim the output voltage but there is always a minimum 4kohm resistance from the ADJ pin to ground.
-Tim