LMZ22005TZ is used 6 times in one of our designs and the same reference U part exhibits a dead short (less than 1 ohm) from the output pin 7 to GND pin 4. This has occurred in 3 CCAs out of 60+. While it is possible (being investigated) that we're inducing the problem during 'SAFE TO POWER ON' tests (continuity/isolation tests), I'd like to know why the datasheet was updated to the effect that one "should be limited to one reflow". What has TI uncovered that lead them to add this new section? In our case we have a few modules on top and a few on the bottom, thus some of these modules would be exposed to two reflow processes. Changing the design is out of the question, so, aside from hand soldering the 2nd side, I'd like to know what's the story on the limited # of reflows to one.
Regards,
V. Mendez
GDLS