Hi Everyone,
Our customer plan to regulate +/- 12V with 1.5A load each from 24V input. I know that The LMZ34002 is appropriate solution for -12V, but now they are considering to use LMZ35003 with inverting configuration. Because they decided to use LMZ35003 for +12V output and so they would like to use the same device both +/-12V. I believe that it can be use with inverting configuration, but now I would like you to advise about layout. And also I'd like to know if LMZ35003 can be used with -12V with 1.5A load from 24V input.
[Question]
- Can LMZ35003 be used with -12V with 1.5A load from 24V input?
- Please see the attached layout and give your recommendation.
LMZ35003 Inverting configuration.pdf
Best Regards,
Sonoki / Japan Disty