I need to upgrade an existing device that uses a PTH08080WAH. I need to increase the max voltage from 18v to 22.2v. Does TI have a module that matches up pin-for-pin but has a higher max voltage? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to upgrade an existing device that uses a PTH08080WAH. I need to increase the max voltage from 18v to 22.2v. Does TI have a module that matches up pin-for-pin but has a higher max voltage? Thanks!
David :
There is no pin-pin compatible replacement for PTH08080W with input voltage greater than 18V maximum limit.
One suggested is to add a pre-regulator on the input voltage bus, Linear regulator, for conversation from 22V to 18V.
If the output voltage for the PTH08080W is 2.5V or more, then a PTN78060WAH(3Amp), not footprint compatible could be used in place of PTH08080WAH.
Any questions, my e-mail is tguerin@ti.com
Tom