Hi Team,
I am using TPS84610 for an application. I need to evaluate the performance of my load without using the DC/DC module. Can I safely connect an external DC source on my output of TPS84610 while holding the INH pin low so that I disable the chip.
I am assuming I will observe a voltage( = output voltage - body diode drop of high side FET) of the chip.
My question is, will this have any adverse effects on the chip given that there are logic and control blocks connected to the input pin.
Thanks!