Hello all,
i am using a PTD08A010W power modul and have a question about the maximum output voltage. The datasheet says 0.7 to 3.6V. But while testing i discovered that the modul is capable to driving higher output voltages, depending on the pulse width of the PWM-input and the input voltage. I generate the PWM with my own circuit.
I only found this in the datasheet: "The maximum input voltage is duty cycle limited to (VO/(130ns × FSW)) or 14 V..."
My question: is the modul capable of driving for example 12V@5A on the output @13V input voltage or are there other restrictions?
Thank you,
Dirk Knoblich