Hello everyone,
I want to use the PTH08T220W to generate a 3V3/10A and another one for a 2V5/3A. A PTN78060WAD will be also used for a 7V/1.45A. All 3 power supplies from a 12VDC.
I would like to know if someone could provide me with those information:
- What is the Ramp ON module characteristics V/µs ?
- What is the maximum Inrush Current available?
- What is the current slew rate (response to a current step) A/µs ?
- What is the maximum current step amplitude ?
In advance, thanks for your help.
Bests regards,