I need dc-dc which is used with battery pack.
Input voltage: 13.2V to 16.8V.
Out1: 12V/5A
Out2: 12V/3A
out3: 5V/3A
Preferably I want to use modules only. I can three different modules if required.
I had checked design for module in webbench, but instead of some module part it gives ic part with ckt & PCB using LM25085.