Is DCP022415D short circuit protected ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is DCP022415D short circuit protected ?
Kaushik;
DCP022415 has an internal short circuit protection.
What is the end application?
Is it IGBT or motor drive application.
My direct e-mail contact is tguerin@ti.com if there any further questions?
Tom
Yes Sir, It is IGBT based application.
We want to measure 1200V DC and Want to Isolate the control From Power Components.
Kausahik:
Product specification : DCP02 series and all other DCP01, DCV01, series cannot meet the isolation requirement for IGBT drive systems.
This application IGBT, requires Basic/enhanced Isolation required for IGBT drive application
DCP02 product specification , page 6, states the maximum continuous working voltage across the isolation barrier is maximum 60VDC and or 42.5V VAC.
See application spec data attached
Tom
dcp020505 page Isolation statement.pdf