Need VID control. Wondering if there's a way to get the LM10011 to work with the PTH08T250W?
How would it be connected?
Thanks,
Dan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Need VID control. Wondering if there's a way to get the LM10011 to work with the PTH08T250W?
How would it be connected?
Thanks,
Dan
PTH08T250W is not compatible for VID voltage control by the LM10011. Recommend a digital DAC control of PTH08T250W output voltage
Tom
Thanks for the feedback.
We have a Freescale/NXP T4240 processor. The core voltage is nominally 1V, 60A with a 3% (±30mV) tolerance through a 20A load step. The voltage also needs to be adjusted at boot time to its VID value.
Are there any examples of using a DAC with a module that you can highlight to show how this might look with the PTH08T250W?