I'm looking for a recommendation on a solution that's beyond WebBench as far as I can tell.
I am looking for a programmable power supply solution.
Input: 5 V
Output: 6 to 15 V, 10 W
Solutions based on modular products preferred.
Shutdown pin preferred
Getting this to work on the first board spin is higher priority than minimizing cost.
To give an idea what I have in mind, at the moment I'm considering using PTN04050C with a DAC controlling an op-amp circuit driving a FET in place of the adjust-pin resistor. However I'm not sure there is enough information available about the internal design of the PTN04050C to guarantee this control mechanism will be stable.