The power supply input is 5V
LMZ3710 is generating 1.8V and 3.3V. The LMZ31506 is generating 1.5V and 2.5V, The LMZ31520 at 1V.
I want to use synch out of an LMZ3710 to drive the RT/CLK inputs of the other LMZ3710 and the two LMZ31506. In looking at the data sheet of the LMZ31520 I will not be able to synch to that part?
In looking at page 26 of the 3710 data sheet you get the resistor values for a given Vout for Rset and R(RT). In my application each part will have a unique R(RT) based on the Vout and switching frequency.. The synch out from the LMZ3710 will connect to the RT_CLK pins to the other LMZ3710 and the two LMZ31606 to make the power control module clock frequencies all the same.
My question is when I synch the three parts to one synch out signal will this synch out clock over ride the internal set frequency (set by R(RT))? Is there a schematic showing how to connect multiple LMZ parts to one clock frequency?
Each part needs to have a resistor from RT_CLK pin to ground that sets the output voltage. T