Hi everyone,
after I soldered this power chip, DCP022405U, which intakes 24V DC and outputs 5V DC, I measured it's output voltage, it was 10.9V, very steady 10.9 volts, please help me figure out the reason.
Here's the condition that might be helpful for you:
- Soldering station: ATTEN 8586
- Soldering temperature: 350 to 380 degrees (C) (I soldered several chips, all output around 10V)
- PCB board layers: 6
Thanks in advance.
Bruce