Hi,
I started using the TPS82130 recently and it works fine, but I had some troubles with getting it operational a couple of times. I set the voltage to 3.3volts with a divider, but only generated 2.04 volts on the output. I resoldered the component to the board, same result. I removed a Ferrite Bead on the input to the regulator and finally got a 3.3Vdc output.
There could have been something else I did to affect this result that I missed, my question is would a 600 ohm ferrite bead affect the regulator in some way?
Input voltage 12 vdc.
Thanks,
Greg