Hi,
My customer is using TPS82085.
Condition is Vin=3.3V, Vout=1.2V, Iout=a few uA.
Please see below waveform.
This is same load which is above condition.
The difference is capacitor value.
Left is 22uF, Right is 44uF.
Customer uses capacitor is JMK212ABJ226MG-T.
44uF is 22uF *2.
I think this situation is PSM mode.
Switching frequency has differance at below picture.
But equation 3 in datasheet does not have element of output capacitor.
Could you let me know the reason of differance of waveform, please?
Best regards,
Shimizu