This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31710: We are getting 3.1V instead of 3.3V at the output

Part Number: LMZ31710
Other Parts Discussed in Thread: TPS3897

Dear Team,

WE are using LMZ31710RVQR to generate 3.3V from 5V .

Enable is controlled through TPS3897 , 

When we check the voltage output it is showing 3.1 in multimetr instead of 3.3V but output waveform is fluctuating between 3.3 and 2V so getting 3.1 in multimeter.(attached vout for your reference)

  

INH pin voltage 2.5V observed.

Please help me us to debug the situation. Why this dip of voltage from 3.3 to 2V in waveform

Regards,

Prasanna G