This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS826951: Bucks understanding if voltage goes below the Vout

Part Number: TPS826951
Other Parts Discussed in Thread: TPS63051, TPS62698, TLV733P, TPS82740B

Hello,

I have sensitive components which have a voltage requirement between 3V to 3.6V. But my battery runs at 3V to 4.2V, I was thinking of using an LDO or Buck converter.

But I was wondering with TPS826951 which is a buck converter if the voltage goes below the Vout would the Buck converter disconnect?

I was hoping if Vout is 3.3V that if Vin goes down to 3V that Vout can go to 3V and not disconnect.

Would this idea work?

Mo