Other Parts Discussed in Thread: CSD18540Q5B, DRV8303, LM46002,
Hi,
we are experiencing similar issues as described in this post: https://e2e.ti.com/support/power_management/simple_switcher/f/858/t/528460
System description:
48V system voltage (Input protection, surge, EMI filtering)
BLDC Motor control with DRV8303 + CSD18540Q5B (halfbridges) + AD8210 (current measurement, 20mOhm)
LM46002 48V system voltage to 12V
LMZ21701 12V to 5V (used for uC [third party 3V3, 1V8 converter], current measurement AD8210)
6 Layer PCB
Top: (Vos trace, ground plane)
Experienced problem:
LMZ21701 works ok as long the PWM on the motor is disabled (ripple ok, output load as specified)
After enabling the PWM on the motor (motor in stop condition, same PWM on all phases) --> Short circuit on LMZ21701 output after ~15min
Things tried already (no success):
- decrease feadback resistors by factor 10
- increase output capacitance (DC bias)
- add small capacitance (100nF) on Vos pin (Top side)
- cutting output 5V traces to trace down noise coupling
- external 12V supply
- and various combinations of the above things
Additional info:
We have a version 1.0 of the same PCB where the "Mid 4" layer do have 5V (on a plane) below the LMZ21701 (48V sys voltage is routed further away) and that version does run and do not have described problem.
How sensitive is the LMZ21701 to noise?