Hi
I got questions from my cutomer.
Could you tell me the following questions?
If the Track terminal is open, are there any problems?
If there are the problems, what does the problems happen?
Best regards,
Yokota
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I got questions from my cutomer.
Could you tell me the following questions?
If the Track terminal is open, are there any problems?
If there are the problems, what does the problems happen?
Best regards,
Yokota
Yokota:
The Auto-Track feature allows the power-up of multiple PTH modules to be directly controlled from the Track pin. However in a stand-alone configuration, or when the Auto-Track feature is not being used, the Track pin should be directly connected to the input voltage,
When the Track pin is connected directly to the input voltage the Auto-Track function is permanently disengaged. This allows the module to power up entirely under the control of its internal soft-start circuitry. When power up is under soft-start control, the output voltage rises to the set-point at a quicker and more linear rate.
Tom
Hi Tom-san
Yokota:
When the track pin is open, the output voltage ramp-up can be non-linear which may effect the external output components
Tom
Hi Tom-san
Hi Yokota-san:
If the track is unused and left open, no connection to Vin 5V, it will only effect is to the Vout voltage ramp-up dv/dt time to regulation. This slow ramp-up time may effect powering -up and sequencing of other external devices placing some power stresses on them.
Attached is fig#1 with open Track control noting over during transition from soft start to open Autotrack control..
Fig #2 is Auto track is defeated by connecting it directly to Vin 5 V.
Tom
.
fig#1 and Fifg#2 see attachment PTH05060W with track conection and no track connection.pdf
Hi Tom-san
Hi