TI Home » TI E2E Community » Support Forums » Power Management » Power Modules » Power Modules - Forum » DCR011205 ripple
Share
Power Modules
  • Forum
  • Announcements
Options
  • Subscribe via RSS

DCR011205 ripple

DCR011205 ripple

This question is answered
Yevgeny Perelman
Posted by Yevgeny Perelman
on Aug 08 2010 08:44 AM
Prodigy20 points

Good day,

Having a large ripple from DCR011205, loaded around 10-20mA. The ripple is some 100mVpp. The datasheet promises

much less than that. Used ceramic X7R capacitors on input/output/recitfier. Any ideas where to look to fix this?

 

Thank you.

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Tom Guerin
    Posted by Tom Guerin
    on Aug 09 2010 11:57 AM
    Verified Answer
    Verified by Tom Guerin
    Mastermind21480 points
    DCR010505 PI filter .pdf

    DCR011205 when  ceramic capacitors on the out bus at 400kHz ripple has a low output  AC component. When  1uf ceramic on the Vrec pin to ground  and 0.1uf ceramic Vout pins to ground the DCR011205 has an average low frequency output ripple of 15mV. The switching , high frequency envelope  , can be higher depending upon the method used to measure ripple and noise. Close coupling across the output  ceramic capacitor at this low amplitude ripple and noise is required for  accurate measurment .  Additional filtering can be added . See attached to reduce  ripple and noise .

    The reflected input ripple and noise can be reduced by adding  PI filter . See attached filter applications diagram.  

    Tom Guerin

    tguerin@ti.com

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Miklos Lammel50528
    Posted by Miklos Lammel50528
    on Feb 23 2012 11:14 AM
    Prodigy60 points

    Dear Tom!

    When I started designing my circuit for DCR011205 I came across your post above, and used your schematic for noise reduction. However now after I have soldered everything together, I have measured with an oscilloscope (PicoScope 2205) the output ripple of the DCR011205, and it is much higher than expected.

    I have attached my schematic, and the measurement results with 68 Ohm load on output of the DCR011205.

    The interesting thing is that if I add a 100nF capacitor between the two isolated ground ( input and output gnd ), then the ripple voltage drops to a fraction (5..10mV which is quite good). Even touching the output with hand ( human body acts kind of like gnd ) the noise drops significantly. This means to me, that the output is kind of  "floating" , but I don't have any idea how to solve this problem. Adding capacitor on output between gnd and vcc did not help. Only thing that has helped, was that I have connected the input gnd and output gnd with a capacitor - but then the hole meaning of a 1000V isolated dc-dc converter is lost.

    Please help me with this issue.

    Thanks,

    Miklós

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Tom Guerin
    Posted by Tom Guerin
    on Feb 23 2012 13:13 PM
    Verified Answer
    Verified by Tom Guerin
    Mastermind21480 points

    Miklos Lammel50528 :

    Thanks for  the ripple  question.  I have several questions

    1. What is the scope bandwidth ? The ideal bandwidth is 20MHz. The scope probe recommended connection   coupling across the  ceramic capacitor. The close coupling removes scopeprobe  ground lead and clip  ( about 7.62cm clip lead)  from the ground probe  barrel. The probe center pin , after   removal of the probe clip )   should be directly connected  to the same  Vout ceramic as the ground barrel < 0.25cm) wire.

    The average output   ripple with the  73 material ferrite bead as PI filter inductor and 2 ceramic capacitors ( 1-2,.2uF) is about 5-10mV when measuring with  close coupling scope probe.   

    The frequency above at 2.59us duration  is about 386kHZ.

     2. On the Sync. pin,  is the sync. pin connected to any component  or is it floating?It is very sensitive to any capacitance

    My e-mail address is tguiern@ti.com . Send me your contact information if you want to discuss this  application.

    Tom  

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Miklos Lammel50528
    Posted by Miklos Lammel50528
    on Feb 23 2012 15:11 PM
    Prodigy60 points

    Hi!

    Thanks for the quick answer!

    My scope has a 25MHz bandwidth and 200Msample/sec Sampling frequency. I have removed the ground lead, and the clip from the scope probe, and magic has happened, the noise is now around 10mV measured 10 cm away from the capacitor on PCB, and 3mV directly at the output filter.

    The frequency is still the same, so I assume that this is the 400kHz switching frequency ( 385kHz is quite close) of the DCR011205.

    The synch pin here in this application is used to synchronise with another DCR021205. If there was no other device, where should this pin be connected if not used?

    And finally a HUGE question arises in me: what is the reason, and the explanation behind this, that removing GND-lead and the clip from the scope probe had such a huge effect on the measurement ?!

    Thanks,

    Miklos

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Miklos Lammel50528
    Posted by Miklos Lammel50528
    on Feb 24 2012 05:25 AM
    Prodigy60 points

    Hi!

    Meanwhile my friends have pointed out that using a Y2 safety capacitor between the two GND lines is a common design practice to reduce EMI. Actually I found, that Linear Tech suggest to use capacitors with their isolated dc-dc converters.

    From the datasheet http://cds.linear.com/docs/Demo%20Board%20Manual/dc1746af.pdf :

    "EMI mitigation techniques used include the following:
    1. Four layer PCB, allowing for isolated side to logic side
    ‘bridge’ capacitor. The bridge capacitor is formed between
    an inner layer of fl oating copper which overlaps
    the logic side and isolated side ground planes. This
    structure creates two series capacitors, each with approximately
    0.008" of insulation, supporting the full
    dielectric withstand rating of 2500VRMS. The bridge
    capacitor provides a low impedance return path for
    injected currents due to parasitic capacitances of the
    LTM2881’s signal and power isolating elements.
    2. Discrete bridge capacitors (C3, C4) mounted between
    GND2 and GND. The discrete capacitors provide additional
    attenuation at frequencies below 400MHz.
    Capacitors are safety rated type Y2, manufactured by
    Murata, part # GA342QR7GF471KW01L"

    So does it mean, that this solution could be used with TI isolated dc-dc converters? Would you recommend it?

    And I would be also very thankful, if you could help me to understand why removing the gnd  lead has helped.

    Regards,

    Miklos

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Tom Guerin
    Posted by Tom Guerin
    on Feb 24 2012 13:05 PM
    Suggested Answer
    Mastermind21480 points

    The long ground lead  and it alligator clip when removed plus the probe  center conductor clip when  measuring across a ceramic capacitor is considered to be close coupling.

    The longer scope ground clip lead which  is typically 7cm long  when it  is attached to any surface or the  robe  is floating reacts as an e-field  antenna. The stray e-field detection when the  scope sensitivity is very high and the bandwidth is at 20 to 25MHZ, will detect any e-mil radiation. The is no power in the e-field .

    I do not think the capacitance type of filter by itself  soes not reqct  by attuating the bus noise.

    Tom

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Tom Guerin
    Posted by Tom Guerin
    on Feb 24 2012 13:22 PM
    Verified Answer
    Verified by Tom Guerin
    Mastermind21480 points
    • The long ground lead  and it alligator clip when removed plus the probe  center conductor clip when  measuring across a ceramic capacitor is considered to be close coupling.

    The longer scope ground clip lead which  is typically 7cm long  when it  is attached to any surface or the  robe  is floating reacts as an e-field  antenna. The stray e-field detection when the  scope sensitivity is very high and the bandwidth is at 20 to 25MHZ, will detect any e-mil radiation. The is no power in the e-field

    The y-capacitance values of  <0.5uF  at 800kHz switching frequencies may not be its reactive frequency range. 1uF and up including 4.7uf  capacitors with X5R tolerance ratings have a low frequency  response. 

    Tom

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • George Ioakimedes
    Posted by George Ioakimedes
    on Feb 29 2012 14:28 PM
    Intellectual910 points

    Just when you thought this thread wouldn't die, I have a few questions:

    1.  If we aren’t going to be using the SYNC pin should I pull it high or leave it
      disconnected?
    2. In your filter design you made up a few years ago you listed a Fair-Rite
      2773021447 part. This part has a max RDC of 0.9mohms which seems extremely low.
      If I wanted to select another part would you have a 2nd choice? Of
      course 0.9mohm is great for keeping the losses low but a quick search on
      DigiKey (for reference) only comes up with some Wurth parts that meet that
      criteria of 0.9mohm.
    3. In your schematic it looks like you’ve got a 0.1uF between Vout and the ERROR pin
      but I think that 0.1uF should be between Vout+ and Vout-, right? And then the
      ERROR pin is just pulled high.

    Thanks,

    George

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Tom Guerin
    Posted by Tom Guerin
    on Mar 01 2012 09:50 AM
    Verified Answer
    Verified by Tom Guerin
    Mastermind21480 points

    George:

    The DCR series or any DCP, DCV series must never be connected to any capacitance.

    1. The sync.. pin must be open with no stray  or capacitance detected by this  pin. orge;

    2.The filter design when using the ferrite bead ( inductor  fair-rite 2773021447 73 material ( ) in PI filter application with 2x 2.2uf  either side  to ground) has a attenuation factor  of 10-15db the 400kHz to 800kHZ primary switching frequency.   I know of no other ferrite bead vendor  which has the high permeability  and resistance of 75-100 or greater  ohms and low frequency range in PI filter application.

    If you Google the  part number, 2773021447, availablility and contacts are listed.  

    3.  The 0.1uf capacitor connection is between VOUT pin to ground. the tie points are (-)vout to (+) Vout) .

    This minimum value for filtering the output bus is 0.1uf.

    Tom   

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • George Ioakimedes
    Posted by George Ioakimedes
    on Mar 02 2012 16:03 PM
    Verified Answer
    Verified by Tom Guerin
    Intellectual910 points

    Tom:

    OK, I've ordered some parts and I think I've got a handle on this but if you could take a quick look at this and provide some feedback I'd appreciate it!

    Thanks,

    George

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Tom Guerin
    Posted by Tom Guerin
    on Mar 02 2012 16:34 PM
    Verified Answer
    Verified by Tom Guerin
    Mastermind21480 points

    George:

    I reviewed the filter and application schematic. The input filter (FB1 ) is I assume the  2773021447 Fair-rite  , 73 material. The output capacitor , C9 ceramic ,should be located  between pin 14 Vout + and FB2. I suggest adding a 1uf ceramic after FB2 and FB3  on load side for complete  PI  filtering .

    Regards

    Tom

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • George Ioakimedes
    Posted by George Ioakimedes
    on Mar 02 2012 16:41 PM
    Verified Answer
    Verified by Tom Guerin
    Intellectual910 points

    Tom:

    Thanks for the quick reply! Yes, C6, C7, and C9 will be placed as close as possible to pins 1, 2, and 14 of the DCR01. So effectively after FB1 on the input side and before FB2 on the output. Yes, those are the 2773021447 beads.

    On the load side, how "bad" would it be to use the same 2.2uF that are on the inputs so as to reduce the number of different components in the BOM?

    Thanks,

    George

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • George Ioakimedes
    Posted by George Ioakimedes
    on Mar 02 2012 18:09 PM
    Verified Answer
    Verified by Tom Guerin
    Intellectual910 points

    Just thought I'd post an updated schematic so if I've got everything correct this time you just say "it looks good"!

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Cedric 40627
    Posted by Cedric 40627
    on Mar 04 2012 11:45 AM
    Verified Answer
    Verified by Tom Guerin
    Intellectual320 points

    Is C11 correctly placed in the schematics ? If yes what is its purpose ?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • George Ioakimedes
    Posted by George Ioakimedes
    on Mar 04 2012 11:57 AM
    Intellectual910 points

    Well to be honest I'm not sure either as I'm not a filter expert and didn't look it up. I was just going off of this statement:

    " I suggest adding a 1uf ceramic after FB2 and FB3  on load side for complete  PI  filtering ."

    which I could very well have mis-interpretted.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
12
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
All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.