I am testing the LMZ313710X2 evaluation board.
I have a issue measuring the correct current across the sense resistors of 1mOhm (R9,R10).
I am using HAMEG HM7042 power supply to supply input voltage of 12V, I set the output voltage via jumper to 1.8V.
I am feeding a external clock input of 300kHz to synchronize two devices on the evaluation board.
I should be reading across the 1mOhm resistor arnd ~8mV-9mV using DMM but get 0 on both devices.
Is there something I am missing tosetup or add for correct operation and test to get desired output currents from devices?
Please advise
Thanks