This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTN78020H: Driving 7A for 25 seconds

Part Number: PTN78020H

For the PTN78020H module, can I do the following?

1. Configure the output voltage for 22V output and drive 7A into the inductive load for only 25 seconds.  The current limit is 8A so I believe I am okay with driving 7A load.

2. I saw that the device has a thermal shutdown mode so is there a way to heatsink the device to prevent thermal shutdown?

Thanks for your help!