This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

low noise and EMI power module or non isolated switcher solution

Other Parts Discussed in Thread: TPS65276V

Hi Guys,

Since I have not yet found what I am looking for I thought I might ask my question in the forum:

I search for a minimum cost/BOM solution for a low noise/EMI PMM solution. So far my results with the WEBENCH are not satisfying. i have the following requirements:

power supply input: 6V(min), 12V(nom), 18V(max):

  1. Load: 2,5V@5,5A(max) --> needs to be low noise for some RF amplifiers (30GHz)
  2. Load: 3,3V@1,5A(max)
  3. Load:-3,3V@0,5A(max)

I think the best approach would be some kind of completely integrated buck converter module with two outputs (one for the 2,5V and one for the 3,3V). For the -3,3V I will use some inverting Rail to Rail OPamps. So far I thought of the TPS65276V. But I don't know if this would be good regarding EMI and low noise. The µModules from linear technology/ADI seem really great but they are pretty exspensive (approx. 30€/pc.). I would be glad if there exist something much cheaper as a solution.

best regards

Benjamin