Hi,
I managed to use the LMZ31520 in an application where I may need to adjust Vout and current limit by a microcontroller.
So I want to use two digital potentiometers for Rset and RILIM;
and my question is :
what are the equations used to calculate both resistors' values.
I can see tables 1 and 6 in the datasheet, but I'll need the equations to acheive more precision (especially for current limitting since table 6 contains only 3 values).
Best regards