This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTV08T250W: question about OTP temperature

Part Number: PTV08T250W

Hello,

There is OTP function on TI's PTV08T250W DC/DC,

but I cannot find the threshold temperature for OTP operation from the datasheet.

And I also wonder the measuring point of temperature.

(The temperature measurement point contents are not listed in the datasheet too.)

please let me know.

thanks,

TS

  • Hi:
    The over-temperature protection is a last resort mechanism to prevent thermal stress to the regulator.
    Operation at or close to the thermal shutdown temperature is not recommended and reduces the long-term
    reliability of the module. Always operate the regulator within the specified safe operating area (SOA) limits for
    the worst-case conditions of ambient temperature and airflow.
    If there are any other questions on the PTV08T250thermals , you can contact me off line at tguerin@ti.com
    Tom