This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82140: Vout setting equation results differs from suggested and Webench solutions

Part Number: TPS82140

Good morning,

I am using this DCDC and I find some problems in the configuration of the feedback resistors.

If I want to configure Vout = 1.8V using the equation given in the datasheet Vout=0,8V*(1 R1/R2)

I get R2=100k, R1=125k. But in the datasheet it is suggested to use 124k. The same says the Webench simulation.

The same thing happens with Vout=1.2V:
I get from the equation R1=50k, R2=100k, and from webench R1=49.9k.

Is it the equation correct? Which values should I trust/use?

thank you very much,
regards
Leonardo