We discovered that the PCB has a via in pad C1 ( Vin ).
Post Assembly we found that Pin C1 was not soldered.
Pin C2 is connected to Vin.
Vin=3.3V ; Vout=5V ; Iomax=75mA.
Question: Pin C1 is connected to Pin-C2 internally to the IC. Since we can not fix the boards
is there a problem with leaving pin C1 floating ??
The Imax for the device is 500mA ... from our analysis Input current
is well in the range ( not even close to Maximum ).
Any comments about possible issues with this build is greatly appreciated.