Hi,
Can you please help me to select the power module or any buck regulator, which is having the below specification.
Vin =24V
Vout =5V
Iout =14V
Thanks & regards,
Divya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi John,
Thanks for your quick support.
We want the regulator which is having internal inductor, i meant to say integrated inductor Like LMZ13610.
Can u please suggest the similar simpler switcher power module.
Thanks & regards,
Divya
Divya:
There are no plans for a power converter with 24Vin 5Vout at 14 amps.
Another discrete solution is the LM3150 simple switcher controller with 17 external components including the external power inductor.
Tom