Customer is testing PTH08T240WAZ for 33℃ condition by thermostatic chamber.
In the case of output current, ①2.33A and ②1.36A.
(Vin: 12V→Vout:5V)
Customer is measured temperature to transformer by thermocouple.
(Condition is continuous 3 hour)
As a result, ② is increased higher than ①.
⇒①:58℃ and ②:62℃
My question is, please let me know about technical reason for ② higher temperature.
I think that larger current should increase higher temperature.
I want to know why temp result became reverse.
(Lower Iout, Higher transformer heat?)
Best regards,
Satoshi