This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31520: power-good functionality in the Forced Continuous Conduction Mode

Part Number: LMZ31520

Hi!

Help me please with one question on LMZ31520.

Is it still possible to have power-good functionality on the PWRGD pin while using Forced Continuous Conduction Mode? I.e., is it correct to have the PWRGD pin pulled up to V5V pin with a 4.7kOhm resistor and the SS_SEL pin connected to the PWRGD pin (for the FCCM) through a 160kOhm resistor (to have 2.8 ms Slow-Start Time)?

Best regards, Vic.