I want to make the output of the LMZM33603 dynamically-adjustable from about 5V to 12V, with a 24V supply. However, I'm not sure what to do about Cff. Making it dynamically adjustable is not really practical (unless it's simple...).
Can I put in a Cff to support the lowest voltage that I'd want to generate? What will that do to the transient response for the higher voltages that would not otherwise need a Cff?
The nominal output load is about 1.5A.
Also, for Cout, to make the 5V to 12V range work I'm looking at 3x 33uF 25V parts, like the C3216X5R1E336M160AC. What do you think of that?
Thanks!