Can the ptn04050c be run in parallel. basically i need the amps of two of these. Or better yet Is there a module that has a 24watt or maybe even 30 watt rating cant seem to find one. At least with a min input of a li ion 2.75 or lower to 4.2 volts or higher. The plan is to have two 18650 2900mah each in parallel. One PTN04050 per a cell 5 volts. my thinking was 2.4 amps x 2 = 4.8 amps total. What i am not sure about is after the ptn04050c's can i just take both outputs to the load without any thing else or would i need some sorta protection on each one. Or maybe if i did this there would be just a big puff of smoke. Seems to me like it would work but i am still pretty much just a slightly advanced noob as far as electronics go. You input is greatly appreciated, Thanks