This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Inductor of LM2587S-ADJ

I have question about inductor of LM2587S-ADJ.

In boost converter,  We think that Rated current of inductor must exceed maximum output current limit(9.5A).

In datasheet p.19, inductor is R4793-A.

Rated current of R4793-A is 4.5A. It is lower than maximum output current(9.5A).

Is it no problem?

Best regards,

  • The inductor should be rated for the current limit; at least 9A.

    The inductor in the data sheet is underrated and is not a good example.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.