Does the On/Off pin on LM2675 part need to be connected?
If it's left floating, is part enabled or disabled?
I couldn't find any information on this in the data sheet.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Just had a quick look on the datasheet:
The apps schematic on p9 and the layout on p22 show this pin as floating.
Hope this helps.
To add to what Mark Green mentioned, if you look at the block diagram in figure 1 (page 7), the EN pin has an internal pull-up current source which gets clamped at 7V. This indicates that the part will be normally ON if the EN pin is left floating.
Regards,
Denislav