Good evening.
I designed a supply-stadio with LM2678-5. I used the follow configuration:
Vinmin = 10,
Vinmax = 40v
Vout = 5v
Iout = 5A
I used WEBENCH tool to calculate the components.
I can have different load so I can have output current variable from 1.0A to 4.5A.
When the load requires low current (1.5A .. 1.8A), When Vin>30v, I have a spike overvoltage (aboout 7v for 100ms) at the moment when I turn on the device.
This overvoltage, often, breaks the LM2678 and they sometimes breaks the load also.
I tried to change the inductor value, the input and output capacitor but I have not found solutions.
I tried to insert the delay between the Vin voltage and ON/OFF signal, but I don’t found solutions.
Do you have some suggestions for me?
Thank you.
Mauro Gatti