Hi all,
I have built an adjustable power supply based on an Lm2576. the specifications are as follows:
Vin = 24V
Vout = 1.23-20V @ 1.5A
The inductor value is 220uH, Cout = 1500uF, Cin = 470uF, R1 and R3 are 1K6 and R2 is a 25k pot.
R1 Connects between one terminal of the potentiometer and ground. R3 connects between the inductor and capacitor junction and the other end of the potentiometer. The pot terminal connects to pin 4 of the regulator.
i have commenced testing this circuit at no load, however have'nt been successfull thus far.
The output voltage swings between around 6V and 1.23V as I vary the pot.
The voltage slowly ramps up to 6V and saturates at that level.
I have tried changing over the regulator and have downsized the output capacitor as well, however the issue was not resolved.
Can anyone please offer any insight as to why this might be happening?