Hi,
I am using the TI evaluation board for the LMZ34002 (TPS84259).
The input is 12V and output set to 3.3V using jumper. Nothing else on the board is changed from factory setting.
For low current loads everything seems fine.
When the load current rises above about 1 amp I see spikes in the output - see the attached image.
What could be the cause of this? Green in input, yellow is output.
Thanks