Is there a recommended connection method between a micro pin and the shutdown line on the LMR14006?
The datasheet mentions that there is an internal pull-up resistor to what I assume is the Vcc for the part. If I leave the line floating or open drain the resulting voltage may be higher then the micro would like. I’m hoping to avoid adding an additional transistor.