Hello,
I would like to use the LMR62014 with a SEPIC configuration.
Vin = 4.5V to 5.5V,
Vout will be adjusted from 3.5V to 8 V (using digital potentiometer).
Iout max = 0.2A
Is it possible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes you can use it in that configuration. Let me dig up a schematic.
Marc