I have used the LM27313 to boost a 5V input to +15V without problem, now I'm wondering whether the same part can be used to generate -15V without any additional components. Can I simply swap the Vout and GND connections as I see done on some other converters (e.g. TPS54620)? Or is there something about the LM27313 that prevents this? Many thanks.