Hi,
We're looking to use a 258x-ADJ part for a triple output supply, using one of the specified Coilcraft/Pulse etc transformers. Question is, the outputs are spec'd at +/- 12V and 5V, and we need to run at about 40% higher voltages - +/-17V, 7V (to get to +/-15 & 5V after LDO regulators). Other than increased current & dissipation issues, is there a reason we can't use the same transformer as spec'd in the 2586 or 2588 datasheet, using an -ADJ part? Thanks.