Hi there
I have designed a circuit using a LM2678-12 that should run 5A, but when I connect even a 700mA load, the output voltage drops to about 9V. Input voltage is 24V.
I am aware that the inductor is only a 3A inductor, but it should still be able to run a load of more than 1A.
The circuit is assembled on a PCB
What is going on? Why would the voltage drop?