1)Fig #31, is a current limit for Vout=3.3V
Can you advise current limit at Vout=4.35V?
2)Will we have 3A version too?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The current limit is not output voltage dependent. You will still see 2A on the valley current as current limit for 4.35 Vout.
Currently we do not have any updates on the 3A version.
Regards,
Akshay
The max current limit is 2.3A at the valley. This means that the valley of the inductor current has to be above 2.3A to trigger the current limit. Once the valley current goes above 2.3A (max limit) then the part enters hiccup mode.
The max peak current limit is 5A. This means that in the hiccup mode, the inductor current could swing up to 5A.
I hope this helps.
Regards,
Akshay