Condition: 9Vin, 7Vout
When there is a load less than 350mA, the output voltage will drop to 5.5V around and then goes up to 7V cyclely. But when load is higher than 350mA, the output voltage will be normally. Please find the waveform as attached. how to improve the problem and what's the limitation? What's the Boostrap's UVLO?
Also, when input voltage goes up to 9.5V, the problem will be gone.
CH1: Vout, CH2: SW pin
Applicaton: automotive
Customer: Whetron-China