Hello,
we usually mount components both on the top and the bottom side of the board.
The board will enter 2 times in the reflow oven. That means that some components will be thermically stressed 2 times.
The oven temperature is the typical temperature of a RoHS soldering process.
QUESTION:
Is the LM43603 controller suitable for a double reflow soldering process?
In other words, will the LM43603 converter be damaged if it enters 2 times into the reflow oven?
Best Regards,
Enrico Migliore